Cancel
Showing results for 
Search instead for 
Did you mean: 

Utilizing CUDA for NX10 rendering tasks

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Helleo everyone!

 

I was asked a question that I'm not sure how to answer. Maybe you can give some advice?

The question is whether NX10 can utilize NVIDIA CUDA technology to reduce time to complete renedring tasks? The specific graphic card in question is NVIDIA FX4000.

2 REPLIES 2

Re: Utilizing CUDA for NX10 rendering tasks

Siemens Phenom Siemens Phenom
Siemens Phenom

CUDA isn't really for rendering. It's a programming interface that lets you use the power of the GPU (graphics processor) for things other than rendering. It only works with nVidia GPUs. If you want to use the GPU for rendering functions, you typically use graphics packages like OpenGL or DirectX. NX doesn't use CUDA, but it certainly uses a lot of the powerful features of the GPU (via OpenGL).

山田
yamada

Re: Utilizing CUDA for NX10 rendering tasks

Experimenter
Experimenter

Hi Yamada,

 

Can we use CUDA programming for make parallel computing with the NX Open API?