Cancel
Showing results for 
Search instead for 
Did you mean: 

VDI with NX and Nvidia GRID

Pioneer
Pioneer

Hello everyone,

 

Actually we are testing VDI deploement with VMware horizon. We have 2 tesla M60.

 

I'd like to know if some of you use this kind of deployment ?

 

And if you have some latency with 3d mouse or rotation with normal mouse ?

 

Or anykind of observation Smiley Wink

 

Best regards

 

Adrien

 

 

 

 

Adrien Marmy, Designer / SystemManager CAx, Turck Interprox

Production: NX12.0.2.mp4 | AGILE PLM E6.1.3 | ECU 3.9.9.3

Development: .NET Testing: NX18**
2 REPLIES 2

Re: VDI with NX and Nvidia GRID

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is a noticeable delay when using a 3D input device.

This might also be a result of too much bandwidth optimization of the horizon software, but we havn't found out the root cause yet.

There are also the new P60 graphics adapters, but we havn't been able to get them for testing and comparing yet too.

If you run this inside a LAN and not a WAN, you could disable any kind of bandwidth optimization, since bandwidth is not an issue inside of a LAN environment.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: VDI with NX and Nvidia GRID

Pioneer
Pioneer

Hi,

 

Thanks for you reply.

 

My IT guys have imporve a lots a setting (I don't have all details yet), like frame rate and also bandwidth as you sugest.

 

We also see that the hardware of the Thinclient had some effect on performance, apparently there is some decompression made from the Thinclient.

 

Vmware will released or alread has, a new update of (horizon... esx... ) and it seems that there is some improvement about this kind of feature (Nvidia Grid performance).

 

I'll keep you in touch end of the week !

 

We can't test P60 hardware compatibilities...

 

 

 

Adrien Marmy, Designer / SystemManager CAx, Turck Interprox

Production: NX12.0.2.mp4 | AGILE PLM E6.1.3 | ECU 3.9.9.3

Development: .NET Testing: NX18**