Cancel
Showing results for 
Search instead for 
Did you mean: 

View Letter Part Navigator Column in Drafting

Genius
Genius

Does anyone know if it's possible to show a view attribute in the part navigator as a column while in drafting?
I want to display the VWLETTER attribute so I can see what view letters are being used more easily.
When I type in the VWLETTER as a column nothing populates, so either it can't be done or I'm doing it incorrectly.

View_Letter.png

2 REPLIES 2

Re: View Letter Part Navigator Column in Drafting

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @Corey1776,

 

It doesn't seem possible.  You also cannot edit the cell in the comment column for which I found the following enhancement request:

ER 7596040 - Adding comment in Comment Column in Drafting application

 

Consider opening an IR with GTAC to request that the view attributes be allowed/readable as columns in the Part Navigator.

 

Regards, Ben

 

 

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: View Letter Part Navigator Column in Drafting

Genius
Genius

That's pretty funny a comment column that can't be used for comments. LOL

I'll write up an IR soon to be an ER.

8978381 - Utilize View Attributes as Columns in the Part navigator for Drafting

 

Thanks!