Cancel
Showing results for 
Search instead for 
Did you mean: 

View NX Licenses- Can I view all License usage from one place?

We have 48 Unigraphics licenses in our office. And the licenses are distributed in 6 servers. If we have to check the license usage, we are running LM Tools in each server. Is there any way to check the uasage of all the 48 licenses from one place?

 

Thanks!

Akshay

6 REPLIES

Re: View NX Licenses- Can I view all License usage from one place?

Valued Contributor
Valued Contributor

Hi,

in your nx-installation-folder you can find the lmutil.exe. You can start it in a command promt on your clinet and send the output to file. In my example the server name ist cad3.

 

c:\plm\nx100\UGFLEXLM\lmutil.exe lmstat -f -c 28000@cad3 > c:\temp\cad3-lm.log

 

You can do this for each of your servers.

 

If you want to find all the used licenses you can use the command

 

findstr "Users of" c:\temp\cad3-lm.log | findstr /V /C:"Total of 0 licenses in use" | sort >> c:\temp\lmsort.log

 

Hope this will help,

Wolfgang

Re: View NX Licenses- Can I view all License usage from one place?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There are also external apps you can try.

Flexera has Flexnet manager (very $$$)

We use another product (I cant find info on them right now)

I'm sure there are others.

I believe someone has a script based usage reporting posted somewhere here in the forums (could be in a legacy forum)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: View NX Licenses- Can I view all License usage from one place?

Thanks Wolfgang!

 

But we need an application which is both user friendly and time efficient. This is because we often exchange license between PCs.

So I was hoping if there was anything out there that could check all the servers at once.

Re: View NX Licenses- Can I view all License usage from one place?

Thanks Ken!

Flexnet manager wouldnt be an option for us, due to the cost.

I'll try to find other products and the script you've mentioned. 

Re: View NX Licenses- Can I view all License usage from one place?

Phenom
Phenom

Siemens document  001-1931728 provides you with some information about

license managers.

There is also a free one, PHP License Watcher, which is no longer mantained

though, we have installed it and IMHO is not worth the effort.

 

Re: View NX Licenses- Can I view all License usage from one place?

Experimenter
Experimenter

Hello Akshai,

 

There is OpenLM which is letting you monitor a your license Server and generating the Data into their Web user interface. You could download an evaluation version from www.openlm.com. 

 

It also contains plenty of other features from receiving Denials, Usage analysis in period of time.... even releasing idle licenses. They also have great support. 

 

Worth a try