Cancel
Showing results for 
Search instead for 
Did you mean: 

View break command on a section view

Valued Contributor
Valued Contributor

Hi,

 

I have a drawing having a view break command on a section view.
This view break makes the section line disappear on the main view with giving error like the below picture 1,

After hitting OK, these lines disappear like the below picture 2,

Is there a way to show the section line again?

 

Thank you,

Regards.

 

1.PNG2.PNG

2 REPLIES 2

Re: View break command on a section view

Phenom
Phenom

Hi @ahmetunkur44,

it's strange this result because the problem is resolved on NX 11.

Are you using NX 10 or NX 11 ?

Try to use the the 'Version Up' command. Use the command finder.

Thank you...

Using NX11 and NX1847 serie
RuleDesigner PDM

Re: View break command on a section view

Valued Contributor
Valued Contributor

Hi @cubalibre00,

 

Thank you for your reply. I am using NX11.0.2 and i didn't come across with this problem again.

I will keep in my mind Version Up command. 

 

Thank you very much.

Regards..