Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

View from drawing or model

Honored Contributor
Honored Contributor

NX 9 with TC 10

 

We use the master model concept, so our model geometry is in one file, and the drawing in another.

 

By default the views are added from the model, but if you do an exploded view, you need to add the fiew from the drawing.   There is/was also some other quirk that I learned from GTAC, and don't recall now, but the work around was to add the view from the drawing.

 

So, my question is, can you set the default to use views from the drawing (specification)?  and if so, is there any drawback to this?

 

-Dave

-Dave
NX 11 | Teamcenter 11 | Windows 10
4 REPLIES 4

Re: View from drawing or model

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm not sure of the answer for this, but...

 

If you apply PMI in the model part, do you have to use model part views on the drawing to inherit/see it?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: View from drawing or model

Siemens Legend Siemens Legend
Siemens Legend

What happens if you don't bother at all ?

 

I would assume that Drafting Development designed NX that way...

- i hope.

 

But, be careful to not get the "drafting components" in the Assembly navigator.

  since they cannot be changed into regular components.

 

Regards,

 Tomas

Re: View from drawing or model

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

From my knowledge, it can only be done via a variable. As per below, the GTAC IR explains why the change from NX8 onwards and how the variable reverses that. I'll caveat, hat it might not work in later versions (I haven't tested for a while).

 

 

IR1943238
Siemens' best practice recommendation for creating drawings is to create
master model drawings. This means the master model resides in one part file
while the drawing resides in another part file.   The drawing file references
the data in the master model file.  Prior to NX 8, when a base view was added
to the drawing, the referenced view would default to the model view from the
current drawing file.  This is counter to the master model best practice.  So
a change to the base view dialog was made in NX 8 to default to the views in
the master model.  Users should be aware of this change and understand the
referenced views and geometry are now of the master model and not what is in
the drawing file.  If users want the pre-NX 8 behavior, they can change the
part option to use the current drawing file and not the master model file or if
they wish to have this as the default for the system they can set the
environment variable

 

<please contact GTAC, referencing the above IR, for this undocumented variable>

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: View from drawing or model

Honored Contributor
Honored Contributor

But if are using master model, what difference does it make for the drawing views to come from the model, or to come from the drawing?  The master model is still the ultimate source for the info.

 

-Dave
NX 11 | Teamcenter 11 | Windows 10