Cancel
Showing results for 
Search instead for 
Did you mean: 

Visibility of measuring points in Daimler Drawing (NX11)

Experimenter
Experimenter

Hallo guys,

 

In an existing drawing, I need to make the 3D measuring points visible. Currently there arrowheads( to show the points) pointing to the approximate locations of the points in drawing. When I use the MODEL final part reference set, only the body is visible and when I use the drawing measuring points Reference sets, only the points and not the body are visible. I need the body along with the points.

 

Thanks in advance for any help you can provide!

2 REPLIES 2

Re: Visibility of measuring points in Daimler Drawing (NX11)

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Check how the reference set is in model.
Most of the time de model reference set is containing only bodies.

if you use entire part you will see everything.
If you go to menu->format->reference set, then can you create a reference set for your self.

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions
Highlighted

Re: Visibility of measuring points in Daimler Drawing (NX11)

Experimenter
Experimenter

Hi Ruud van den Brand,

 

I am sorry for the late reply...Daimler have a lot of different reference sets....They also a reference set for measuring points...however I have no idea how to make that particular reference set to make visible in a view with the measuring points.  But many thanks for your help!

 

Regards,
Saty