Cancel
Showing results for 
Search instead for 
Did you mean: 

Visualization Settings in Siemens Nx

Experimenter
Experimenter

Hi,

I am using Siemens Nx for surface modelling. Now i am facing a problem regarding visualization. Eventhough after sewing the sheets i donot have any gap between surfaces, i can see them visually. But according to siemens, there are no gaps and the gaps are under specified tolerances. But i donot want to see those gaps below tolerances visually. How can i change the visualization setting?

1 REPLY 1

Re: Visualization Settings in Siemens Nx

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It could be a result of your faceting settings. Try the following to see if it helps: go to menu -> preferences -> visualization -> faceting; change the facet scale to "view" and turn on the "align facets along edges" option.