Cancel
Showing results for 
Search instead for 
Did you mean: 

Washer with corner down rounded corner

Experimenter
Experimenter
Can anyone tell me the method of making down corner as image of washer attached?
Is there any command in nx for that, because i already had many sheet metal parts( not limited to washer or fastner) like this one
6 REPLIES

Re: Washer with corner down rounded corner

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @anshu1986,

 

Do you mean like this?  Using sheet metal you can get the flattened blank correct with perpendicular edges, then use the bend feature.

2018-06-12 10_42_35-Siemens NX - Sheet Metal.jpg

There are of course so many ways this can be achieved.

 

Dave

Re: Washer with corner down rounded corner

Experimenter
Experimenter
Not like this one. Actually pls have look of image again from bottom and top.
Its a sem screw with washer if u want more pic of it

Re: Washer with corner down rounded corner

Siemens Phenom Siemens Phenom
Siemens Phenom

@anshu1986 wrote:
Not like this one. Actually pls have look of image again from bottom and top.
Its a sem screw with washer if u want more pic of it

I was offering you a generic method as you stated

 


@anshu1986 wrote:
because i already had many sheet metal parts( not limited to washer or fastner) like this one 

The image of the washer is clear and not something that is typical for the sheet metal application, this is more like a pressing.

Dave

Re: Washer with corner down rounded corner

Experimenter
Experimenter
Any other method for modeling

Re: Washer with corner down rounded corner

Phenom
Phenom

What is the purpose for the model?

 

  • A rough representation to create realistic images of an assembly?
  • To design the stamping tooling in the manufacturing of your washer?

Do you design and manufacture these washers, or just use them in an assembly?

Re: Washer with corner down rounded corner

Phenom
Phenom

@MarkLawry

I have the same questions as Mark.

If you aren't manufacturing these parts, a representation is probably all you need. Otherwise you are cluttering your assembly with non-essential geometry which can add up if you are including a lot of these in an assembly. "Add up" as in graphics rotation calculations, drawing view generation, etc.

Similar case is those users that feel they have to model threads on hardware..just because you can doesn't mean you should!