Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Wave link body dependencies

Valued Contributor
Valued Contributor

Hi!

 

I have some linked bodies in part that I use to make it dependent on the others part dimensions. I've changed assembly structure and got links broken. Unfortunately when I "Edit with rollback" linked bodies and select the same geometry that I've selected before the structure change, I have all my dependent features broken (planes).

Is there a way to make link bodies work again without editing every feature that was using this body?

 

nx_links.JPG

2 REPLIES 2

Re: Wave link body dependencies

Siemens Phenom Siemens Phenom
Siemens Phenom

When you edit the wave link and have selected the body click on the Mapping Replacement Assitant.

If you have not change the parts onyl the structure then setting Matching Algorithm to Geoemtric and doing a find should patch the faces and edges correctly, simple tick and accpet the matches.

 

Steve V

Re: Wave link body dependencies

Valued Contributor
Valued Contributor

It's worked, thanks.