Cancel
Showing results for 
Search instead for 
Did you mean: 

What does this error message mean?

Builder
Builder

"The record area asked for does not exist in this object"

 

I have done a 'Save As' of an existing file to use as the base for another design. As I was trying to remove features that I do not need from this file, I was faced with the above error as I tried to delete a non-needed Sketch.

 

Can anyone help me with:

1) Explaining the error message

2) How do I fix the underlying issue so that I might be able to delete the Sketch.

 

A Part Cleanup had no affect on the message.

 

Thanks!

1 REPLY

Re: What does this error message mean?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Send it to GTAC. I've reported one of these for a customer before and in our case it was a corrupt part that was fixed by GTAC.
Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2