Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

What is the nomenclature TEXT1 <D1><F2><C2.000>TEXT2<C><D><F>

Valued Contributor
Valued Contributor

Hello 

 

TEXT1 <D1><F2><C2.000>TEXT2<C><D><F> Where TEXT1 is not formatted, TEXT2 is formatted

 

In Nx11 detailing we are formatting the text height using the above codes.

 

Here i need to understand the D1, F2, C2.000, C, D and F.

 

Can anyone explain this.

 

Thanks in advance.

 

Sekar

3 REPLIES 3

Re: What is the nomenclature TEXT1 <D1><F2><C2.000>TEXT2<C><D><F&gt

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Sekars 

Refer NX help documentation "Using control characters to format text"

Re: What is the nomenclature TEXT1 <D1><F2><C2.000>TEXT2<C><D><F&gt

Siemens Phenom Siemens Phenom
Siemens Phenom

@Sekars ,

 

C: Character Size.
C2: 2 will be the number controlling the size (which you change to control text size).

D: Character Line Width.
D1: 1 is the line width. 
F: Font type.
F2: 2nd font location in the font list.


Adding <C><D><F> at the end will reset all setting to default and so any text after this will have default formatting.

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: What is the nomenclature TEXT1 <D1><F2><C2.000>TEXT2<C><D><F&am

Valued Contributor
Valued Contributor

Thanks to both Ganesh and Samadhan

 

Your replies help me to find the options by using the Letters and number in the coding terminology.

 

Thanks again.

 

Sekar