Cancel
Showing results for 
Search instead for 
Did you mean: 

What is the nomenclature TEXT1 <D1><F2><C2.000>TEXT2<C><D><F>

Genius
Genius

Hello 

 

TEXT1 <D1><F2><C2.000>TEXT2<C><D><F> Where TEXT1 is not formatted, TEXT2 is formatted

 

In Nx11 detailing we are formatting the text height using the above codes.

 

Here i need to understand the D1, F2, C2.000, C, D and F.

 

Can anyone explain this.

 

Thanks in advance.

 

Sekar

3 REPLIES 3
Highlighted

Re: What is the nomenclature TEXT1 <D1><F2><C2.000>TEXT2<C><D><F&gt

Siemens Phenom Siemens Phenom
Siemens Phenom

Re: What is the nomenclature TEXT1 <D1><F2><C2.000>TEXT2<C><D><F&gt

Siemens Phenom Siemens Phenom
Siemens Phenom

@Sekars ,

 

C: Character Size.
C2: 2 will be the number controlling the size (which you change to control text size).

D: Character Line Width.
D1: 1 is the line width. 
F: Font type.
F2: 2nd font location in the font list.


Adding <C><D><F> at the end will reset all setting to default and so any text after this will have default formatting.

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: What is the nomenclature TEXT1 <D1><F2><C2.000>TEXT2<C><D><F&am

Genius
Genius

Thanks to both Ganesh and Samadhan

 

Your replies help me to find the options by using the Letters and number in the coding terminology.

 

Thanks again.

 

Sekar