Cancel
Showing results for 
Search instead for 
Did you mean: 

Where is Adjust Minimum Radius command of NX 12 (Reverse Engineering)

Creator
Creator

Hi everyone
I saw "NX 12 Convergent Modelling Demos" and i can see the command "Adjust Minimum Radius" on demo movies (see picture), But I can't see it on my work station. If who are used this command already, please reccommend me.

 

Note : my information
- NX Version: NX 12.0.0.27
- NX: Patch None
- OS: Version Windows NT (x64) 6.2 Windows 8 Pro (Build 9200)

 

Adjust Minimum Radius.jpg

3 REPLIES

Re: Where is Adjust Minimum Radius command of NX 12 (Reverse Engineering)

Siemens Phenom Siemens Phenom
Siemens Phenom

Eid, sorry about this, that command did not make it into the production release. The movie was created before that command was removed from the software. We are hoping to be able to get it into the software as soon as possible.

 

Scott

Re: Where is Adjust Minimum Radius command of NX 12 (Reverse Engineering)

Creator
Creator

Hi Scott

Thank you for your explain.

 

Re: Where is Adjust Minimum Radius command of NX 12 (Reverse Engineering)

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

add this moment you can use the smooth to make the sides better but not to a minimum radius just like the movie.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions