Cancel
Showing results for 
Search instead for 
Did you mean: 

Where is the drafting sheet revision letter

Experimenter
Experimenter

My company uses "-" for the initial release of a drawing sheet.  The drafting sheet revision does not allow "-".  Where is the list of acceptable "letters" defined?  I would like to modify this customer setting to allow the use of "-" as a sheet revision.

2 REPLIES 2

Re: Where is the drafting sheet revision letter

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Teamcenter or Native?

What is the current revision if not "-"?

 

Note if the current revision is "0" (zero)...

In tabular notes there is a "zero display option", which allows you set the display of zero to "-" (or a couple other options).  Would this work for you?

 

Ken

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Where is the drafting sheet revision letter

Experimenter
Experimenter

I'm working both Teamcenter and native.  The sheet revision setting I'm looking for is to control what is an acceptable "letter" in the Edit Sheet menu (right click on the drawing sheet in the Part Navigator.

My sequence of "letter" changes are "-", "A", "B"..."AA", "AB", "AC"...