Cancel
Showing results for 
Search instead for 
Did you mean: 

Why won't NX keep my custom Studio Material

Honored Contributor
Honored Contributor

I took one of the OOTB studio materials, and adjusted the color RGB values, applied it, and saved the part.  Now, it seems everytime I open the file, that color is junk, reset to something of no use, so I have to do it over again.  It's been awhile since I've done any rendering, so I was wondering what am I missing?

-Dave
NX 11 | Teamcenter 11 | Windows 10
2 REPLIES 2

Re: Why won't NX keep my custom Studio Material

Siemens Phenom Siemens Phenom
Siemens Phenom

I think you'll find that the custom materials are saved in the work part.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Why won't NX keep my custom Studio Material

Honored Contributor
Honored Contributor

That's what I expected, and I'm working within a single part.  The file is an assembly, but I have waved the bodies i want to render into this single file.  When I copy Car Paint Blue, and modifiy the RGB to be the color I want, and rename it, it remains in the file, but the values and settings go haywire.

 

The Studio materials I copy, and do not change the RGB values, but only change the name, so I can identify what part it is for, everything remains intact.  Customizing the color itself seems to cause the issue.

-Dave
NX 11 | Teamcenter 11 | Windows 10