Cancel
Showing results for 
Search instead for 
Did you mean: 

Wrap Image on Surfaces Not Using Advanced Studio (NX 11)

Experimenter
Experimenter

Is there other tools outside the Advanced Studio to wrap or project an image on surfaces? 

 

I'm looking into something similar to the decal feature, but don't want to 

2 REPLIES 2

Re: Wrap Image on Surfaces Not Using Advanced Studio (NX 11)

Phenom
Phenom

Hi @RobertLHeureux,

there isn't alternative solution.

Thank you..
Using NX1880 and RuleDesigner PDM

Built-in functions for converting units of measure

Highlighted

Re: Wrap Image on Surfaces Not Using Advanced Studio (NX 11)

Valued Contributor
Valued Contributor
Hi @RobertLHeureux
Could you tell us what you need to achieve?
You could use a dxf to project line onto your surface with the flattening and forming tool.