Cancel
Showing results for 
Search instead for 
Did you mean: 

Zoom direction change

Experimenter
Experimenter

Hi,

 

I installed the NX11 and my problem is that i hade used the CTRL+MMB to zoom in and out. The function was that up was zoom out down zoom in. That changed in NX11.  Is there an option to change this?

Pls Help this drives me Crazy

5 REPLIES

Re: Zoom direction change

Siemens Phenom Siemens Phenom
Siemens Phenom

Sorry i might not have understood your query properly but can't you use this for adding your own shortcut?

zoom.jpg

 

Best Regards

Kapil

Re: Zoom direction change

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Tauform,

With the default keyboard/shortcut settings, Ctrl+MMB or scrolling the MMB wheel can be used to zoom in and zoom out.


The function was that up was zoom out down zoom in. That changed in NX11.  Is there an option to change this?

What change did you see in NX 11 about this?

 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: Zoom direction change

Siemens Phenom Siemens Phenom
Siemens Phenom

Thanks Ganesh,

i think i got your issue now...but i too could not find any changes in NX11 in the behaviour of CTRL+MMB for zoom-in zoom-out

Best Regards

Kapil

Re: Zoom direction change

Valued Contributor
Valued Contributor

Is it about changing direction of the zoom?

 

Re: Zoom direction change

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Customer defaults -> gateway -> view operations -> view operations -> mouse wheel scrolling direction. This option controls the direction of zoom for the mouse scroll wheel and also the ctrl + MMB. You will need to change this option and restart NX for it to take effect.