Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

a group of parameters multiplied by a factor?

Genius
Genius
I have more than 20 parameters set as constant numbers (e.g. p21_x = 50). 
 
Is there any easy method to get all those parameters multiplied by the same factor?
 

For example, with a factor 1.1,

  • p21_x = 50   >>>   p21_x = 55
  • p22_x = 60   >>>   p22_x = 66
  • ...
 
All those parameters are "Total" in Curve Length features. I don't want to set them as expressions like p21_x = 50*factor, because I need them to be constant numbers to be able to be adjusted by mouse dragging in the future.
 
Thanks!
 
Image.png
2 REPLIES 2

Re: a group of parameters multiplied by a factor?

Siemens Phenom Siemens Phenom
Siemens Phenom

Go into the expression editor and Ctrl C copy into buffer

Open Excel and past into spreadsheat

Enter factor in another cell

in column next to first orginal number type in formula (cell to left * the factor cell , fixed with $$)

Copy cell to rows below

Copy answers into buffer

Go back to NX and paste new numbers back in.

 

Steve V

Re: a group of parameters multiplied by a factor?

Genius
Genius

Hi @StevenVickers   Thank you for the super trick!