Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

advanced plot gets "Cannot Access Plot Server"

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

User reported this in NX7.5, but it effects NX10 as well.

File -> Plot -> expand "actions" click on "Advanced plot"

I get an error dialog "Cannot Access Plot Server"

 

If I try anything else that ends up displaying an SDI dialog (File -> Utilities -> Printer Administration -> pick a group; or directly running %UGII_BASE_DIR%\nxplot\nxplotadmin) that doesn't work either.

 

I do have an IR open, but i'm wondering if someone figured this out already?

 

I've done some playing with Java (I didn't have java 8 to begin with, I was 7r71, tried 8r102 and 8r31 with no success)

 

Any ideas?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


1 REPLY 1

Re: advanced plot gets "Cannot Access Plot Server"

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In case anyone else encounters this...

Nextlabs Endpoint Enforcers v8.2 appears to be the culprit

 

Ken

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled