Cancel
Showing results for 
Search instead for 
Did you mean: 

"Component is Reference - only" hidden in drafting

Experimenter
Experimenter

Hi,

 

I am using NX11 and TC 10. 

I have added few assemblies consisting of 100's of componentes in DRAWING specification, but when I am adding the BOM it is selecting all the parts from the navigatior. I am not able to make the components as REFERENCE ONLY because it is hidden. How to activate the option of "Component is Reference - only" in drafting environment.

4 REPLIES 4

Re: "Component is Reference - only" hidden in drafting

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
when do you have this dialog in the drafting application or in modeling application?
Some settings that are affecting the assembly structure are only possible to edit when you are in modeling and not possible when you are in drafting

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: "Component is Reference - only" hidden in drafting

Experimenter
Experimenter
Thank you Ruud Van den Brand

Understood, so any other alternative?
I don't want to use EDIT LEVEL command in the part list and deselect 200-300 parts.And I am not using parasolid reference because most likely the model geometry keeps changing and this way I can avoid replacing parasolid every time.

Re: "Component is Reference - only" hidden in drafting

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

you can also set an attribute in the part properties to ignore in parlist.

ignore partlist.JPG


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: "Component is Reference - only" hidden in drafting

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @SD1325,

 

You cannot make a 'component' one-level-down from the specification a Reference Component.  Add the assembly to your master model as a component and you will be able to use this option.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration