Cancel
Showing results for 
Search instead for 
Did you mean: 

angle between a curve and a surface

Valued Contributor
Valued Contributor

I'm looing for an efficient way to confirm the tangency between a curve and a surface. As tought by @TimF in a previous post, this is key for the success of Thru Curve Mesh.

 

Below is a simplified model. The four edges of the Green face are all tangent to the neighbouring faces. Now let me try to measure the angle between the highlighted edge and Face_A.

 

Method 1

At first, I simply use "Simple Angle" to measure the angle between the edge and the face. The result "113.3380°" is apparently not what I expect (180°).

 

Method 2

Then I try to do it step by step:

  1. linear extension of the edge
  2. project the extended line to Face_A
  3. linear extension of the projected curve
  4. measure the angle between the two extend lines
  • The result "0.000014°" is OK.

I wonder whether there is a better way to measure the angle between the curve and the face or simply to test their tangency. Thanks!

 

I tried "Deviation Checking" > "Edge to Face", but was confused about how it works. Official documentation provides very limited information about the command.

 

Image.png

 

Image.png   Image.png

2 REPLIES

Re: angle between a curve and a surface

Siemens Phenom Siemens Phenom
Siemens Phenom

Datum Plane, select along edge of green surface. Change location on curve to 100% and cycle orientation on curve to be binormal to path.

Intersect curve between surface a and plane.

measure anglbe between edge and curve.

 

Steve V

Re: angle between a curve and a surface

Valued Contributor
Valued Contributor

Hi @StevenVickers  Thanks!

 

Your solution based on binormal plane should be the right method to do the job.

 

My method based on linear extension and projection should be wrong!