Cancel
Showing results for 
Search instead for 
Did you mean: 

arc command

Experimenter
Experimenter

hi, what is the quickest way to draw an arc tangent to end of two exixting lines (radius is not known). I can't use the sketch since it is a 3D path.

Thanks

4 REPLIES

Re: arc command

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Can you please share an image of the same if possible? I can think of circular blend curve but not sure if it works for you.

Regards

Kapil

Re: arc command

Genius
Genius

Hi,

 

if it is a real 3D Path than an arc can't work, because an arc must be planar to be a real arc. For 3D you can use the Circular Blend Curve to get a bridge curve based on a cylinder. The result would be the closest form to analytic geometry.

 

Regards André

Re: arc command

Phenom
Phenom

Unable to play video. Please try again later.
(view in My Videos)

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: arc command

Experimenter
Experimenter

hi, thank you for the aswers.