Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

assembly

Valued Contributor
Valued Contributor

Is there a way to apply limitations to assembly part movement. Example: If my assembly were a vice , I would like to set limits on the travel of the clamping mechanisms. Basically when I slide the moving clamping part it would stop moving in the closing direction when 2 specific surfaces make contact.

3 REPLIES 3

Re: assembly

Phenom
Phenom

No, only starting to NX 11.

Thank you...

Using NX1867
RuleDesigner PDM

Re: assembly

Valued Contributor
Valued Contributor
Thank you. I thought about it, and started to wonder if I were to write an expression for the value of a distance constraint, if that might work, what do you think?

Sent from my iPhone

Re: assembly

Siemens Phenom Siemens Phenom
Siemens Phenom

@SR

You can define additional assembly arrangement and make the distance constraint as arrangement specific. Here you can use an expression while specifying the distance constraint as arrangement specific.