Cancel
Showing results for 
Search instead for 
Did you mean: 

assembly

Valued Contributor
Valued Contributor

Is there a way to apply limitations to assembly part movement. Example: If my assembly were a vice , I would like to set limits on the travel of the clamping mechanisms. Basically when I slide the moving clamping part it would stop moving in the closing direction when 2 specific surfaces make contact.

3 REPLIES

Re: assembly

Phenom
Phenom

No, only starting to NX 11.

Thank you...

Using NX11 and NX1847 serie
RuleDesigner PDM

Re: assembly

Valued Contributor
Valued Contributor
Thank you. I thought about it, and started to wonder if I were to write an expression for the value of a distance constraint, if that might work, what do you think?

Sent from my iPhone

Re: assembly

Siemens Phenom Siemens Phenom
Siemens Phenom

@SR

You can define additional assembly arrangement and make the distance constraint as arrangement specific. Here you can use an expression while specifying the distance constraint as arrangement specific.

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New