Cancel
Showing results for 
Search instead for 
Did you mean: 

associative alternative to Divide Curve?

Genius
Genius
  • Divide Curve → non-associative 
  • Divide Face   → associative 
  • Split Body     → associative
Is there an associative alternative to Divide Curve? Thanks!
7 REPLIES

Re: associative alternative to Divide Curve?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

i don't now for sure that there is any associative divide/split feature for a curve.

 

What i do sometimes is to make a surface of the curve, then split/divide the curve and after that i use the edges of the divide sheets to use further in the design


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: associative alternative to Divide Curve?

Genius
Genius

Hi @ruud_vandenbrand   Thanks for sharing your workaround!

 

Generally I would create a short line at the dividing point on the curve and then select the partial curve with "Stop at Intersection" for other operations.

 

I can't understand why only Divide Curve is designed to be non-associative.

Re: associative alternative to Divide Curve?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Divide body used to be unassociative; meaning it would remove all parameters from your file, leaving you with 2 dumb bodies. Trim curve used to be unassociative only until recently. I wouldn't be surprised if there was an associative divide curve option in a future release of NX. Have you contacted GTAC to open an enhancement request?

Re: associative alternative to Divide Curve?

Genius
Genius

Hi @cowski1  Thanks for your information! Then the development team should be aware of the issue, and there must be certain difficult situation to improve it.

Re: associative alternative to Divide Curve?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

They may be aware of the issue, but filing an IR/ER would make them aware of your NEED for the enhancement.

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: associative alternative to Divide Curve?

Siemens Phenom Siemens Phenom
Siemens Phenom

Starting NX11.0.1, the Trim Curve dialog now has a Trim or Divide section where you can change the Operation to Divide.  Given this, you should be able to figure out how to associatively divide the curve.

 

Trim Curve Enhancements (11.0.1)

 

Regards, Ben

Re: associative alternative to Divide Curve?

Genius
Genius

Hi @BenBroad   Thanks! It's exactly what I'm looking for.