Cancel
Showing results for 
Search instead for 
Did you mean: 

associative dimension not updating

Pioneer
Pioneer

NX9

I'm using associative measure to set the length of a deformable part in an assembly arrangement. Sometimes when I change the arrangement, the associated length in the Part Navigator doesn't update, even though the dimension on the assembly window is correct, and as a result, my deformable part doesn't update. I have to double click the Distance Measure feature, click OK, then everything updates. Is there a way to force the distance expression to update without reopening the feature?

4 REPLIES

Re: associative dimension not updating

Pioneer
Pioneer

This might help explain my problem. After changing my Assembly Arrangement, the true distance is 15.200mm but the Part Navigator will continue showing 10.500mm and the deformable part (spring) will not change.

 2017-04-13_13h06_23.png

Re: associative dimension not updating

Builder
Builder

Hello@AICLE

 

try out this

 

Menu>Tools>update>update for external change

 

this cmd work for me for accociative measure /analysis

 

i think it should be work either you have to contact GTAC for the issue.

 

thanks

Warm Regards
Thomas Roman
Machine Designer

Re: associative dimension not updating

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @AlCLE,

When you switch between the arrangements, component position changes, although you have associative measurement it will not update for the deformed part. Double clicking the measurement distance in part navigator shows the message about the change in the position of the objects that has been used while creating the associative measurement. 

 

measure.PNG

 

I have attached a video as an example. In assembly I have used two arrangements, in second arrangement I made distance constraint as arrangement specific and defined the expression for it. Whenever I change the component position in either arrangement it needs update to reflect the changes in the other arrangement for the deformed part. As you know already, double click measurement in part navigator or use 'Update for External Change' as @Thomas_Roman mentioned to update the deformed component with respect to the arrangement defined.

 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: associative dimension not updating

Pioneer
Pioneer

Thanks for the replies. "Update for external change" works but takes a while as it updates nearly 800 features.