Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

associative feature copy

Creator
Creator

Hello citizens,

 

In IDEAS you could use FEATURE COPY to associatively copy features within a part.  This was useful when patterning or mirroring wouldn't work.  Pro-E has PASTE SPECIAL which if I remember right, does the same thing.  NX has PASTE SPECIAL but it's non-associative.

 

In NX how can you associatively copy a feature like a boss or pocket and place it somewhere else on the part?  I tried different things and did some research, but I don't see any easy way to do it?

 

How is everyone out there handling that?

 

Thanks in advance,

 

Alex

7 REPLIES

Re: associative feature copy

Siemens Genius Siemens Genius
Siemens Genius

Hi AlexHouston,

You can create "User defined feature". With help of it, you can insert boss/pocket/custom feature associatively into other part

Tools > User Defined Feature.

 

Thanks,

Amol

 

Re: associative feature copy

Phenom
Phenom

Look into the NX Reuse library! Plenty of functionality packed into that tool.

Re: associative feature copy

Phenom
Phenom
Oh, and there is a simple copy/paste too. Ctrl+c and ctrl+v. Or you have patterning.

Re: associative feature copy

Creator
Creator

What I ended up doing is using an associative extraced feature command and then moving the extracted body (using point to point) to a new location point.  The body is still associative to the to original, so that is what I'm trying to do, but it is there a cleaner method?

 

 

Re: associative feature copy

Gears Phenom Gears Phenom
Gears Phenom

Have you tried looking into pattern geometry, or (Feature)?  Set the layout option to general, Then you can copy the geometry from point to point or from a Coordinate system to Coordiante system. 

 

Re: associative feature copy

Creator
Creator

That is exactly what I was looking for!  I was able to slap features anywhere I had place points and add features on the back side of the part by adding a CSYS in first!!!

 

I never knew that general tab was there.  I only did linear or circular patterns.

 

Thank you kind sir!

Re: associative feature copy

Experimenter
Experimenter

Thank you very much AlexHouston and !

 

As a long time Creo (Pro/E) user this is exactly the functionality I was looking for in NX - CSYS to CSYS associative move/copy using Pattern Geometry [General].

In my case I also had to change the orientation in the Orientation section of the dialogue to “Follow Pattern” (default is “Same as Input” - Thanks Glenn!) because I had both linear and rotational offsetting of the destination CSYS.

 

Best regards!