Cancel
Showing results for 
Search instead for 
Did you mean: 

backgrounds, color combinations

Pioneer
Pioneer

Hello,

 

  • Is there a particular combination (backgrounds, color) that protects the eyes? (less exhausting)

 

  • Can you create the colors according to the user? And also open this color combination, even if someone else has drawn a part with different settings?

 

 

Thanks,

Linda

 

 

5 REPLIES 5

Re: backgrounds, color combinations

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @BachmannL,

You can edit the background color as per your choice from

Menu > Preferences > Color Paletter or

File > Preferences > Background

 

You can customize, save the CDF file which can be used to override the default color palette of NX.

Overriding the color palette

 

Default 'ugcolor.cdf' can be located in the UGII folder.  

 

 

Re: backgrounds, color combinations

Pioneer
Pioneer

Hello @GaneshKadole,

we still have NX10.
When I open a component of a colleague from the USA e.g., I see his color palette.
Is it possible that I always see my standard no matter who drew the component?

Re: backgrounds, color combinations

Siemens Phenom Siemens Phenom
Siemens Phenom
 
 
You need to open part/component, load/open the required CDF file from 'Color Palette' dialog and save the part so that new color palette will be saved with the part.

Re: backgrounds, color combinations

Pioneer
Pioneer
@GaneshKadole,

ok well then i can make a macro and just start this with every part needed.

Thanks Smiley Happy

as "eye-friendly Colors" would you recommend the standard NX dafault cdf?



Highlighted

Re: backgrounds, color combinations

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

I recommend the usage of Visualization Templates. Because it could also be that you do not only want to change the palette, but also other viusalization settings.

see Link to Documentation

 

Regards,

Johannes