Cancel
Showing results for 
Search instead for 
Did you mean: 

ballooning in NX8.5

Experimenter
Experimenter

Is there a way to line up all called out balloons at once horizontally or vertically in NX 8.5?

11 REPLIES 11

Re: ballooning in NX8.5

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Of you use the selection filter you can select the balloons faster and use then the horizontal or vertical group feature

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: ballooning in NX8.5

Experimenter
Experimenter

Thank you for your reply.

But if i use the horizontal group feature,the balloon leader goes missing. I have attached  a picture showing how I  need it with the leaders but to be horizontally lined up with some space in between.

 

Re: ballooning in NX8.5

Phenom
Phenom

Hi @Prajwal_P,

what you ask it's not possible. Please insert an ER and add here the number, so we can be added.

This is a feature interesting that lack, like other feature in the explosion environment. 

Thank you...

Using NX1867
RuleDesigner PDM

Re: ballooning in NX8.5

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

When placing callouts, I like to turn on the "grid" and "snap to grid" options. This makes it super easy to line up balloons.

Re: ballooning in NX8.5

Experimenter
Experimenter
What is ER?? I didn't get you. I am new to this..please be kind..

Re: ballooning in NX8.5

Siemens Phenom Siemens Phenom
Siemens Phenom

@Prajwal_P wrote:
What is ER?? I didn't get you. I am new to this..please be kind..

ER -  Enhancement Request

 

From NX 8.5, Go to Help > Online Technical Support > Log an Incident with Technical Support.
For this you need to register with a valid webkey which can be found at Help > About NX > System Information > Webkey Access Code.

 

Also take a look at this blog article

You submitted your IR/ER/PR… Now what?

 

 

Re: ballooning in NX8.5

Valued Contributor
Valued Contributor

I think Siemen's has already stopped support of new issues in NX8.5.

| NX 8.5.3          |     December 31, 2015     

Re: ballooning in NX8.5

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If current versions still have the issue, you can still log an IR

If you log an IR and the issue is "fixed" in a newer version of NX, they can tell you what version it was fixed in (subject to the versions they have available - e.g. if the older version they currently have access to is NX10, they might say "it was fixed *by* NX10", without being able to say if it was actually fixed in NX9 or NX10)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: ballooning in NX8.5

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

@jadodaro wrote:

I think Siemen's has already stopped support of new issues in NX8.5.

| NX 8.5.3          |     December 31, 2015     


Correct (well,.. almost).  GTAC continues to support all versions (as they have done so in the past) whereas development will only support versions up to their maintenance end dates: NX End of maintenance support

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration