Cancel
Showing results for 
Search instead for 
Did you mean: 

broken links beetwen 2D and 3D model in assembly draft

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi everyone, 

 

I have problem with assembly draft. I lose links beetween 2D nd 3D model. I can not update some sheets, because I lose links. Ia attachment I add some screenshots. Anyone is able to help me?2d_links_broken.jpg2d_2.jpg

 

best regards

lukipap

1 REPLY 1

Re: broken links beetwen 2D and 3D model in assembly draft

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @lukipap,

 

That icon to me looks like the view was created as a "Snapshot" view, used to prevent a view from updating.  Expand the Part Navigator to see the "Up to Date" column and hover over the icon for the views - you should get a tooltip showing that they're snapshot views.

 Screenshot - 2_6_2018 , 8_47_35 AM.png

To disable this setting, right click the views and choose "Settings".  Under "Common > Configuration", check to see if the Lock Method is set to "Snapshot".  If it is, change it to "None" and see if that corrects the issue.

 Screenshot - 2_6_2018 , 8_49_26 AM.png

Regards, Ben