Cancel
Showing results for 
Search instead for 
Did you mean: 

change revision NX

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi everyone, 

 

I need to change revision in draft  2D in draft table but I am not sure how I can do it. There are some atributes responsible for that? I hope you are able to help me. 

 

Best regards

lukipap

 

 

2 REPLIES 2

Re: change revision NX

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Guessing...(you aren't too clear on what you are looking for)

- you have a drawing

- in the title block (somewhere) there is a "Revision" field

- you want to update that field

 

1) Is that field filled in by an attribute?  or just manual text?

- if manual text, you have to edit it manually

2) If an attribute, which one?
Note there can be a revision of the PART, or a revision of the drawing SHEET.

 

Drawing sheet revision is controlled by the sheet (right-click on the border, or the sheet in the PNT, -> edit sheet -> somewhere on the dialog is a "revision" field.

 

Part revision is typically (in Teamcenter) the DB_PART_REV attribute, and controlled by TC.

Native mode, there is a way to define revisions (for load options) but I don't know if that revision is available as an attribute inside NX.

 

I'm not fond of using the drawing sheet revision for the rev, as each sheet could then be at a different revision.  But if that is your company standard, go for it.

 

Hope something in the above helps you out...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: change revision NX

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @lukipap,

 

OOTTB, the sheet revision is driven by the system attribute: <W@$SH_SHEET_REVISION>.  This text field is embedded in a Title Block definition on Layer 256.

To change the value, right click on the sheet in the Part Navigator and choose Edit Sheet and enter in your desired Revision:

 

Screenshot - 6_6_2017 , 7_39_50 AM.png

 

Regards, Ben