Cancel
Showing results for 
Search instead for 
Did you mean: 

change text height within a note

Pioneer
Pioneer

In drafting, is it possible to change the height of text within a note?  For instance, I might want the text to be 6 mm tall for one word and then 4 mm tall for the remainder of the note.  Thanks.

3 REPLIES

Re: change text height within a note

Gears Phenom Gears Phenom
Gears Phenom

You can change it by a factor, or 2x, or .5x, etc. (in red box), which adds the bit of code in the text (underlined)

 

TextSize.jpg

-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Re: change text height within a note

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

To accompany @DaveK's reply, here's the relevant page in the documentation:

Using control characters to format text

 

Regards, Ben

Re: change text height within a note

Pioneer
Pioneer
Thank you.