Cancel
Showing results for 
Search instead for 
Did you mean: 

change units

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi,

two questions: (NX11.0.2) I need to get Body Measurements so that the volume is in cm3 and the weight is in g: is it possible?

Second question: The Help doc says you can set the variable UGII_UNITS_WRITE_FILE, to be able to store new units into a file. But in the env file I didn't find this variable: shall I simply add it to my customized env file? 

Thank you

 

2 REPLIES 2

Re: change units

Siemens Phenom Siemens Phenom
Siemens Phenom

Laurus --

 

First question:

 

[Dropdown] Menu --> Analysis --> Units [at the very bottom] --> g - cm

 

Done.  :-)

 

Second Question:

 

Yes.  I just put mine in my NX startup script.

 

Does that help?

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com

Re: change units

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

thank  you!