Cancel
Showing results for 
Search instead for 
Did you mean: 

checking of thickness of a solid on the fly

Pioneer
Pioneer

hello all, i used catiaV5 before and it has a function in the measurement command that you can check the part thickness on the fly also the flatness of the face, is the same thing possible in NX too? checking the surface is flat or not is really painful, any solution on this?

19 REPLIES 19

Re: checking of thickness of a solid on the fly

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

you can use "Face curvature analysis" to check the flattness of a surface

And use "check wall thickness" for the thickness check.

 

these checks are not included in every bundle of NX


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: checking of thickness of a solid on the fly

Pioneer
Pioneer

True a "Face curvature analysis" is ok but i have to select the face and run the analysis that's painful because i need it frequently but in catia it used to be i just select a command and it displays the flatness with a plane symbol next to it, i cant find something like this

i can compromise on thickness as it is less frequent, but a similar tool is available in catia to perform the task

Re: checking of thickness of a solid on the fly

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

maybe visual report can help also with this.

(view in My Videos)


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: checking of thickness of a solid on the fly

Pioneer
Pioneer

@ruud_vandenbrand thanks for the video mate!!!

but as u see this method is ok for a simple block, where in i have a complex geometries of a automotive bumper and lots of reinforcement parts, this method is ok but takes a hell lot of time.!!!

if you have used catia u will know, its lot easier

Re: checking of thickness of a solid on the fly

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

did you tried to type in the Catia command in the NX command finder?


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: checking of thickness of a solid on the fly

Pioneer
Pioneer

ya the first thing i did Smiley Sad

 

Re: checking of thickness of a solid on the fly

Pioneer
Pioneer

if not i need to parse the pointer location and print it on the label via NXOpen program development i might try this.!!!

Re: checking of thickness of a solid on the fly

Gears Phenom Gears Phenom
Gears Phenom
@MrX,

You might want to look into Deviation Gage and make sure you're quite familiar with NX Selection filtering to make things go faster so that you're not picking each face one at a time whenever possible.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.6

Re: checking of thickness of a solid on the fly

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @MrX,

 

I realize you're not using NX12, however, you might be interested to learn about the new Thickness Analysis functionality starting with NX12.0.1 mp1.  With the Measure dialog open, use Object to select the solid body and then with Point selected, use the Point on Face option to select a point on the face of the body to see a dynamic thickness displayed.  You can then drag that point around the entire body:

 

(view in My Videos)

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration