Cancel
Showing results for 
Search instead for 
Did you mean: 

color part problem

Pioneer
Pioneer

Please guys, I have big problem to a color set up, although in basic set up is turned on a grey color (as defaut) still I have some orange color as you may see on picture bellow. How can I solve it? Just to notice you that isn't a default setting, I get it after I fixed something what I can't remember and even how I did it.color problem.PNG

11 REPLIES 11

Re: color part problem

Valued Contributor
Valued Contributor

Any chance something is selected in the part history in the part navigator window?

 

Re: color part problem

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Do you think this is the result of having selected something and now it can't be deselected?  If that's the case (and hitting the Escape key on the keyboard doesn't work) try selecting: "File > Utilities > Part Cleanup" - check "Remove Extraneous Highlighting" and hit OK.

 

Regards, Ben

Re: color part problem

Phenom
Phenom
You are showing an assembly. You could either have the parts colored in each respective file, or you could have the components colored in the assembly, overriding each part color. You can select all the components in the assembly; Right-click; and select Edit Display. Then select the color.

Re: color part problem

Legend
Legend

Hi @IloveAudi86

 

If you means default color of solid body at creation time,

you can set it from [Preference > Object].

Chose Type (solid body) and specify color.

 

(Most of Preference setting is part specific. And default setting is come form Template part. )

 

 Sunkap Ahn, Senior Support Engineer


logo

Re: color part problem

Hello,

 

If it is a assembly,disabling the 'Specific Component Color' will bring back the original Part Color.

Specific.PNG

Thanks and Regards,
Mathi Krishnan.

Re: color part problem

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Something else to consider:  Synchronize Subassembly Properties

 

(view in My Videos)

 

Regards, Ben

Re: color part problem

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

@IloveAudi86 - did you get this resolved?

 

Regards, Ben

Re: color part problem

Pioneer
Pioneer

Hi Ben! I can`t work on computer on which I have problem. As soon I start to work on i would follow your instruction. And I will notice you.

thank you

Re: color part problem

Pioneer
Pioneer

No, I did that but not solve the problem. But thank you i think Ben's solution is OK. And sorry you wait on my answer so long.