Cancel
Showing results for 
Search instead for 
Did you mean: 

colour spill and slowing NX

Pioneer
Pioneer

My computer configuration is old but I know it can do better than this. Now, from some reason, when I move the cursor accross any part in assembly it start very boring color spilling and last 10-25 seconds. I'm sending an ilustration of that and my configuration. Thank you.3.PNG6.PNGkonf.PNG

4 REPLIES 4

Re: colour spill and slowing NX

Gears Phenom Gears Phenom
Gears Phenom
I could be wrong, but graphics card and driver information might be useful in addition to the above.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1

Re: colour spill and slowing NX

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I've seen this in a few cases:

 

1) Unsupported graphics card.  See here for certified hardware:

https://www.plm.automation.siemens.com/en_us/support/gtac/certifications.shtml

 

2) Old/bad driver

 

3) If you have built-in Intel graphics on laptop, sometimes NX chooses to use this graphics chip instead of the certified card.  If you have NVidia, try using the Nvidia control panel -> Manage 3D settings -> Program settings -> Select Siemens NX and "lock" it to the NVidia graphics card.

 

Hope this helps...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: colour spill and slowing NX

Phenom
Phenom

I think what you are seeing is the result of some of the Selection Preferences on a non-supported graphics card.

Experiment with  turning off these Selection Preferences.

 

selection_preferences.jpg

Re: colour spill and slowing NX

Pioneer
Pioneer

I did it. It helps but there is a small problem: it won't mark part when the cursor is on it (or right over it). Thank you very much.