Cancel
Showing results for 
Search instead for 
Did you mean: 

conecting drawing templates in NX 12

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi!

I can not add my template of drawing in NX 12. I upload here  whole "template" folder from following path:E:\Program Files\Siemens\NX 12.0\UGII\templates. I have change files, which I have also upload here. When I try to chose new drawing there is  no templates to chose, the same as on the picture, which i upload as well. I hope will you able to help me, because it is really bursting my job.

 

pic of error.png

 

Best regards

Lukipap

mobile:+48  694867888

2 REPLIES

Re: conecting drawing templates in NX 12

Gears Phenom Gears Phenom
Gears Phenom

Did you edit the templates.pax file?

 

 

Re: conecting drawing templates in NX 12

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
The NX12 drawing templates are now stored in the following folder:
%UGII_BASE_DIR%\DRAFTING\templates

The script only imports templates that reside in the folder defined in the script, so you will have to consider copying your drawing templates into that folder.

Regards, Ben