Cancel
Showing results for 
Search instead for 
Did you mean: 

constrain poles of a 3D spline as in 2D sketcher?

Genius
Genius
To manipulate 3D splines seems to be tricky for me. Below is an example:
 
Is there an easy way to associatively constrain the 6 poles of the spline to the 6 sketch points in axis Y direction? In other words, if the 6 spline poles are projected to XZ plane, the resulting points would be exactly conincident with the 6 sketch points. 
 
The idea is borrowed from 2D sketch. I'm not sure the workflow is reasonable or not. Hope to have your suggestions.
 
Thanks!
 
Image.png
 
Image.png
3 REPLIES

Re: constrain poles of a 3D spline as in 2D sketcher?

Siemens Phenom Siemens Phenom
Siemens Phenom

 

Hi @surfactant

I made a solution that measures your original spline poles from the Y constant plane and creates contruction curves from the sketch points down along Y at the measured values. Then make a new spline through the end points of the construction curves.

Probably more complicated than you hoped for and I'm sure your real model is more complicated. This can be easilty automated with some code to make it super effecient.

Regards

Paul

(view in My Videos)

 

Re: constrain poles of a 3D spline as in 2D sketcher?

Genius
Genius

Hello

 

you can create construction lines through the sketch points and normal to the sketch plane. Then you can use the end points of the lines to create a associative spline.

 

3d-spline_based_one_sketch.PNG


Meinolf, , Leistritz Turbinentechnik GmbH


Production: NX10.0.3, TC 10.1.4

Testing:NX11 Beta

Re: constrain poles of a 3D spline as in 2D sketcher?

Genius
Genius

Hi @Triumphator  @Paul_Hartrick   Thank you both for your solutions!