Cancel
Showing results for 
Search instead for 
Did you mean: 

conversion of a Pattern geometry Subtype Helix to Helix curve

Valued Contributor
Valued Contributor

Hello Dear friends in my pracise I have came up across a bit of a strange case.

see attached file for more details

 

regards from bulgaria

2 REPLIES

Re: conversion of a Pattern geometry Subtype Helix to Helix curve

Siemens Phenom Siemens Phenom
Siemens Phenom

If you first get the values from the pattern geomtery, you can then just plug the "p" values into the helix command. I think this is the question you are asking. See the image below, I got the values I needed from the part navigator and then used them in the helix command.

 

Helix.pngHelix expressions

 

Scott

Re: conversion of a Pattern geometry Subtype Helix to Helix curve

Valued Contributor
Valued Contributor

the answer is very helpfull thank you a lot for it.altho my point was is there a nother way besides that one that you pointed out