Cancel
Showing results for 
Search instead for 
Did you mean: 

create streamline

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi.

 

I want to make a streamline.

 

streamline.jpg

 

Is there a way?

7 REPLIES 7

Re: create streamline

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Sorry perhaps i was not able to get your question properly. 

Is it something related to machining?

If you need only curves in modeling then can you use this option ?

 

 

iso.jpg

 

Best Regards

Kapil

Re: create streamline

Siemens Phenom Siemens Phenom
Siemens Phenom

If this is a CAM question, it should be asked here.

 

NX Manufacturing Group

 

Thanks,

Scott

Re: create streamline

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

No.

 

I want to make curve line.

Re: create streamline

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

ISO Curve is ..

 

iso_curve.jpg

Highlighted

Re: create streamline

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

The isoparametric curve gives you straight line because the original patch is planar (the curved boundaries are the result of trimming the surface ).

In that case you need to use offset curve in face.

Best Regards

Kapil

Re: create streamline

I'm confused. The original picture shows a tool path, so as @ScottFelber says, we have a forum for that. If this is about creating geometry, then it belongs here. Do you want this post moved to Maufacturing? 

 

Mark Rief
Retired Siemens

Re: create streamline

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Thank you.

 

The original picture shows a tool path. But I would like to leave it in curve like toolpath.

 

Is not there a way?