Cancel
Showing results for 
Search instead for 
Did you mean: 

creating a FCF with horizontal text, flag leader - NX10

Creator
Creator

I'm trying to create a feature control frame for an angled surface, but I want the text to be displayed horizontally and not in-line with the surface.  But, when using the "feature control frame" button in the Annotation tab, the FCF is always in-line with the surface when using the Flag leader.  The second pic shows how I want the FCF displayed (horizontally); I had to fudge this with a sketched line and moving a FCF to be in-line with it.

 

I tried adjusting the lettering angle in settings (which didn't do anything), and I tried transform (ctrl + T) to no avail.

 

Is there any way to do this properly?

 

Thanks,

WRM

 

 

4 REPLIES

Re: creating a FCF with horizontal text, flag leader - NX10

Siemens Phenom Siemens Phenom
Siemens Phenom

Hold Shift key while creating FCF and check the resulting orientation.

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: creating a FCF with horizontal text, flag leader - NX10

Creator
Creator

Maybe I'm doing something wrong, but after I specify what I want the specifics of the FCF to be in the dialog window, I click "flag" for leader and then click "select terminating object".  But, when I depress the shift key, it won't allow me to select the surface that I want to associate the FCF with.  Once I release the shift key though, it will allow me to select normally.

 

Am I supposed to hold down the shift key at a different point in the process?

 

Re: creating a FCF with horizontal text, flag leader - NX10

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

The way to get the desired appearance is to use a Plain leader attached to the dimension line with the arrowhead set to none.

 

Flag leaders will always force the FCF to align with the angle of the attachement object.

Re: creating a FCF with horizontal text, flag leader - NX10

Creator
Creator

Thanks Marc; that works!