Cancel
Showing results for 
Search instead for 
Did you mean: 

creating multiple associative points

Valued Contributor
Valued Contributor

hello eveyone,

 

I want to create multiple associative points based on the coordinates in an Excel File. I want to be able to change these coordinates by Excel any time. How can I do this?

6 REPLIES 6
Highlighted

Re: creating multiple associative points

Gears Phenom Gears Phenom
Gears Phenom

Reuse Feature with multiple associative csys or a sketch containing points and constrained somehow will give you that functionality.

Or simply a Sketch with points (constrained to x, y, z) and you can simply import the expressions from spreadsheet.

Re: creating multiple associative points

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

you can use UG_cell_Read in the expressions.

Make for every point a X,Y,Z expression and link the to a cell 

 

after changing the excel use the "update for external Change" to update the part file.

 

only if it are a lot of points it can take some time

 


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: creating multiple associative points

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Using a sketch in this instance assumes that all the points lie in the same plane...

Re: creating multiple associative points

Valued Contributor
Valued Contributor

Thank you all for solutions but there are more than a 100 points on the same plane. Is there a faster way to do this? I’ve already tried the approaches commented above

Re: creating multiple associative points

Valued Contributor
Valued Contributor

Thank you for your replies. I figuredi it out . Video in the attachment

 

(view in My Videos)

Re: creating multiple associative points

Siemens Phenom Siemens Phenom
Siemens Phenom

Great solution,

 

 

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com