Cancel
Showing results for 
Search instead for 
Did you mean: 

crooked section view in NX

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

 

I want to create section view from existing section line but new view is crooked as on attachment. Do yu have any idea to solve it??

 

draft.jpg

7 REPLIES 7

Re: crooked section view in NX

Siemens Phenom Siemens Phenom
Siemens Phenom

If you need the revolved section view projected to the base view, set the 'Hinge Line' vector direction correctly.

 

sectionline.PNG

 

sectionline1.PNG

 Just edited the image to highlight the hinge line option.

 

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New

Re: crooked section view in NX

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

but I do not have 'hinge' method in this dialog window. Check attachment pls.hingemethod.png

Re: crooked section view in NX

Siemens Phenom Siemens Phenom
Siemens Phenom

I am seeing it in both NX 10 and NX 11, your image looks like it is still using the section line for the hinge line. Move up and define a new hinge line first and then see what happens. Also di d you reset the menu?

 

Scott

Re: crooked section view in NX

Honored Contributor
Honored Contributor

Look one section up, in the "Hinge Line" section of the dialog.

-Dave
NX 11 | Teamcenter 11 | Windows 10

Re: crooked section view in NX

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
yep, sorry - my false.

best regards Smiley Happy

Re: crooked section view in NX

Phenom
Phenom

Hi,

I've the same problem.

I would like that the section view is rotated so line become vertical. I need to rotate the view or during the section dialog I'm able to set correctly ?

section view.png

Thank you...

Using NX11 and NX1847 serie
RuleDesigner PDM

Re: crooked section view in NX

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

hi, check answer above. yiu must have specified vector.