Cancel
Showing results for 
Search instead for 
Did you mean: 

default temp directories in NX

Builder
Builder

Hello@Experts

 

currently i am facing new error in NX

 

like this image,can you give me suggestion for this ,,

 

temp dir in NX.JPG

 

 

appreciated for help

Warm Regards
Thomas Roman
Machine Designer
2 REPLIES

Re: default temp directories in NX

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Typically NX uses the folder specified by the ENV variable "TMP" (not "TEMP") (or the "Start in" folder) for the temporary file folder.

 

In NX, do a File -> Help -> Log File

 

Search for "ugii_tmp_dir"

 

compare to the OS level env variable "TMP"

 

Do you have write access to this folder?

 

Note it could be changed in an env.dat file (see if UGII_ENV_FILE is set by searching the log file)

and/or the "Start in" folder could be set differently based on the "start" shortcut used to start NX and/or a .BAT file used to start NX.

 

The next time this happens, if you look in the log file, it may display more info about what specific folder it is having problems with.

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: default temp directories in NX

Builder
Builder

Hello@Ken_A,

 

thanks dude for information

 

thanks again

Warm Regards
Thomas Roman
Machine Designer