Cancel
Showing results for 
Search instead for 
Did you mean: 

dependency of General Conic

Valued Contributor
Valued Contributor
  • "myLine": vertically above X axis, center point on Z axis
  • "SKETCH_000": two points on Y axis
  • "myConic": constrained on XY plane, start/end points = ends of "myLine", interior/anchor points = "SKETCH_000" points 
I'm surprised to find "myConic" has no dependency on "myLine"! Do I miss something? Or this is the nature of General Conic? Thanks!
 
ScreenClip [2].png
 
ScreenClip [3].png
2 REPLIES

Re: dependency of General Conic

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

The line used as a reference for the conic does not lie in the plane that you have constrained the conic to. NX "temporarily" projects the line end points onto the plane to construct the conic; in your dialog for the conic, you can see that the end points are "fixed", which means NX used the current (unassociative) location in time & space. If you want the line to drive the conic, try using "project curve" to create an associative copy of the line (or at least its end points) on the same plane as the conic. Use the "in plane" objects to drive the conic end points.

Re: dependency of General Conic

Valued Contributor
Valued Contributor

Hi @cowski1 Got it. Thanks!