Cancel
Showing results for 
Search instead for 
Did you mean: 

dimension break lines spesific case

Valued Contributor
Valued Contributor

Hello dear colauges.greetings from bulgaria.today i had a very unusual question by my supervisor about a very spesific function that was used for many years in our company.it's the custom symbol for line break GAP25 and GAP125.unfortunately we have moved to NX10.and here the drafting settings for dimension line break a quite different.how ever my question is.Is there a way to break a dimention line when it intersekt with a dimention annotation from a nother dimention.i have a picture as a attachment.

dimentions are marked the orange dimention needs two brakes that are indicated.the yelow dimension annotation text overlaps the orange dimention line.

 

how can this spesific case be resolved.

 

2017-09-21_204942.png

6 REPLIES

Re: dimension break lines spesific case

Legend
Legend

In the ISO standards, it is actually against the rules to break extension or dimension lines for any reason.  ASME standard allows it one one scenario only.

Re: dimension break lines spesific case

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

in the settings of an annotation you can create a Breaks

Create_break.JPG

Right click on the dimension that needs to have the break->Line/arrow->Break->format

Here you can set the Break on or off and the break size.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: dimension break lines spesific case

Siemens Phenom Siemens Phenom
Siemens Phenom

Breaks get create if extension lines/leaders overlap with each other. It does not create a break if the leader and displayed dimension value overlaps as shown by @Aleitin.

 

Re: dimension break lines spesific case

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Space out the dimensions so that they do not overlap. Breaking this dimension as shown will only cause confusion.

Re: dimension break lines spesific case

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Aleitin!

In NX 10, still you can use GAP25 and GAP125 symbols.

Search for the command 'User Defined Symbol' in drafting application.

 

uds.png

 

Re: dimension break lines spesific case

Valued Contributor
Valued Contributor

THANK YOU FOR THE REPLY THAT WAS THE SOLUTION THAT I WAS LOOKING FOR