07-28-2016 08:27 AM - edited
Hello,
how it is possible to manage the line length (below). I'm not find the parameters in customers default.
Thanks
Emmanuel
Solved! Go to Solution.
07-28-2016 08:48 AM
you can find the setting in the Drafting Standard -> Annotation -> Line/Arrow (register) -> Dimension Arrow Out Length Factor
regards André
07-28-2016 09:11 AM
Hello André,
I have also testing this parameter without succes. You are not in NX10?
Thanks.
Emmanuel.
07-28-2016 09:29 AM
My picture is from NX 9. But I've tested it in NX 10 (NX 10.0.3.5 MP6) too. And it works:
But I created a new part. Maybe it doesn't work with existing parts directly. Try to Load the changed Drafting Standard:
07-29-2016 02:37 AM
Hello André,
it is well this parameter. but it is not possible to change a dimension already performed.
Thanks.
07-29-2016 02:47 AM
You're right. The Setting works only for new dimensions. Even an inherit doesn't work.
Regards André