Cancel
Showing results for 
Search instead for 
Did you mean: 

display both knots and UV curves for a surface?

Genius
Genius
I just find that, for a surface, if "Show Knots" is on, UV curves can't be displayed in Wireframe mode.
 
Do I miss something? Thanks!
 
Image.pngShow Knots" ON
Image.png"Show Knots" OFF
 
Image.pngIn Alias, the knots (curves) are displayed as solid, and the UV curves as dotted.
2 REPLIES 2

Re: display both knots and UV curves for a surface?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Surfactant,

 

Youre not missing anything. Its a way of decluttering as the curves often tend to hide eachother making people confused. The IsoCurves appear when needed e.g. when in I-Form (see picture below). Aside form that most people are working in shaded mode (I believe) where Knots & Poles are avaiable - is there a need for combining? Do you have a workflow requiring that?

 

2018_05_31_01_20_16_NX_12_Modeling.jpgBest Regards

Fred

Re: display both knots and UV curves for a surface?

Genius
Genius

Hi @Sandman   Thanks for your reply!

 

I just noticed that Alias users work mainly in the Wireframe mode. They generally depend on UV grids (dotted) and knot lines (solid) to monitor the flow and the structure of most surfaces closely. I think the workflow is good for class A surfacing. That's why I have the question in the original post.