Cancel
Showing results for 
Search instead for 
Did you mean: 

display degree/segment of selected curve/surface?

Genius
Genius
In Alias, they have a status box indicating the degree/spans of the selected curves or surfaces. The box can also be used to edit the values instantly.
 
I wonder whether there is any workaround to get similiar function in NX, without turning on Show Poles and Show Knots for each. Simply displaying the values instantly, without editting capability, is OK.
 
Thanks!
 
Image.pngAlias
2 REPLIES 2

Re: display degree/segment of selected curve/surface?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Surfactant,

 

In NX we do this by using X-Form. Colaps the menu to only show Parameterization if you like the Alias behaviour - expand the menu if you want to unleash the mutitude of editing capabilities.....

 

2018_05_31_08_09_11_NX_12_Modeling.png

 

Best Regards

Fred

Re: display degree/segment of selected curve/surface?

Genius
Genius

Hi @Sandman   Thanks for your reply!

 

I'm just thinking about..., if there is something like a status bar instantly indicating the parameters of the selected curve/surface, it would be a very helpful guidance for all kinds surfacing operations, not just the sculpting operations like X-Form. No problem, I would settle on current NX functionalities. Thanks!